AnsweredAssumed Answered

JN5169 programming connections

Question asked by Pierre Le Gargasson on Sep 11, 2018
Latest reply on Oct 3, 2018 by Pierre Le Gargasson

Hello,

I plan to use JN5169-001-M00-2Z modules as end devices without any carrier PCB. I am thinking about a programming solution.

1 - Does a hardware programming tool exist ? I mean, hardware connect the module inside the tool. Flash the module. Disconnect the module from the tool.

2 - Does a connector reference exist for the module form factor ?

3 - Programming datasheet tells to connect UART0 pins. Can I only connect RX/TX ? Or RTS/CTS are needed too ?

 

Thanks for your help. Regards.

Pierre

Outcomes