AnsweredAssumed Answered

PRH600 TX1 (32) & TX2 (30) Max Output Voltage

Question asked by Luis Sandoval on Sep 11, 2018

Hello,

 

Could you provide infomation about the max output voltage and current that TX1 and TX2 outputs can achieve?

 

VDD is connected to +5V. Additionally, a 125KHz Antenna (600uH; DC resistance < 25homs) is connected from TX1 to TX2 with DC blocking capacitors.

 

Any information you could provide will be really appreciated.

 

Best regards,

Luis Fernando Sandoval.

Outcomes