OM26630FDK board RF Field ON-after reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM26630FDK board RF Field ON-after reset

461 Views
wizardek
Contributor I

Hi, 

I have a question regarding  a board OM26630FDK with the NFC chip CLRC663. I would like have RF Field active every time. Now I am using NFC Cockpit and when I select RF Field On....RF field is active but when I reconnect the USB cable. RF field  is deactivated. And I want RF field permanently working after connection to the power supply. 

BR,

Tomas 

Labels (1)
0 Kudos
1 Reply

355 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

In this case, a program which executes this specific behavior shall be developed and flashed. Please refer to the following link for the NFC Reader Library. There are some helpful examples to take as a base for your project:

NFC Reader Library|NXP 

Happy development!

Regards,

Ivan.

0 Kudos