Is there any good sample in read/write device internal registers on I2C bus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any good sample in read/write device internal registers on I2C bus?

834 Views
a_mazraee
Contributor I

Hi everybody.

I have study all examples about the LPI2C applications in iMXRT1052. But there is not any implicit approach that could address and modify devices internal registers contents which has been connected to the processor with #I2C bus. 

Is there anyone who could help me to find out the best approach to use LPI2C for doing that?

Thanks in advance.

Tags (2)
0 Kudos
1 Reply

701 Views
igorpadykov
NXP Employee
NXP Employee

Hi A Mazraee

one can look at mcuxpresso EVK-MIMXRT1050 examples:

Welcome | MCUXpresso SDK Builder 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos