Hello there
I am debugging the es8323 audio chip on imx6ull
The operating system is linux4.1.15
The driver is sound/soc/fsl/imx-es8328.c and sound/soc/codecs/es8328.c
Found that imx-es8328.c requires device tree configuration audmux, but there is no menuy maps on imx6ull
How should I do it?
The i.MX6ULL SoC doesn't include the AUDMUX module. Moreover, there seems to be no pre-built support of the ES8328 audio codec on the i.MX6 platform.
Thank you for your reply
But this driver is available in sound/soc/fsl/imx-es8328.c and sound/soc/codecs/es8328.c
So I think imx6ull should support es8328
and there seems to be no pre-built support of the ES8328 audio codec on the i.MX6 platform. What means?
Has anyone debugged es8323?