MKE04Z8VTG4 Memory Map and Missing region in Linker File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKE04Z8VTG4 Memory Map and Missing region in Linker File

453 Views
LukeJ
Contributor II

Hi, I was recently looking at a co-workers project and he was out of flash space.  Upon reviewing the output memory map file, the user manual for the MCU, and the linker file, I noticed that the flash in range [0x00C0, 0x03FF] is shown as part of the flash region in the manual (and never otherwise mentioned), but not accounted for in the linker file and the output .map file does not show that region being used.  His linker file was generated by Processor Expert, but I created a dummy project with that part using IAR and that linker file also did not account for the flash in that region.

As a result, I added the region m_text2 to his linker file and moved some code to that space.

MEMORY {
  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000000C0
  m_text2      (RX) : ORIGIN = 0x000000C0, LENGTH = 0x00000340
  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x00001BF0
  m_data       (RW) : ORIGIN = 0x1FFFFF00, LENGTH = 0x00000400
  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
}
...
  .lowFlash :
  {
    . = ALIGN(4);
    *database.o (.text .text*)           /* .text sections (code) */
    . = ALIGN(4);
  } > m_text2
  /* The program code and other data goes into INTERNAL_FLASH */
  .text :
  {
    . = ALIGN(4);
    *(.text)           /* .text sections (code) */
    *(.text*)          /* .text* sections (code) */
    *(EXCLUDE_FILE(*database.o).text .text*)
    *(.rodata)         /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)        /* .rodata* sections (constants, strings, etc.) */
    *(.glue_7)         /* glue arm to thumb code */
    *(.glue_7t)        /* glue thumb to arm code */
    *(.eh_frame)
    KEEP (*(.init))
    KEEP (*(.fini))
    . = ALIGN(4);
    _etext = .;        /* define a global symbols at end of code */
  } > m_text

Is there a reason that this memory range (more than 10% of available flash memory on this part) is not accounted for in the default linker files?  Is it safe to use these addresses as done above?

Thanks

0 Kudos
1 Reply

377 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Lucas Jeanmaire

There isn't any special reason to not include this part of the flash in the main code, it is common for kinetis devices to start the code after the flash config section (0x410).

I don't see any problem in the linker file that you use.

Regards

0 Kudos