Hello, to make it short,
1) I have a signal with cat dev/input/touchscreen0
2) I have installed tslib in my imx6qsabreauto board
3) With ts_calibrate command, it doesn't make below files (I only have a ts.conf file)
TSLIB_CONSOLEDEVICE
TSLIB_CALIBFILE=/etc/pointercal
TSLIB_CONFFILE=/etc/ts.conf
TSLIB_PLUGINDIR=/usr/lib/ts
4) With ts_test_mt, it does work well with touchscreen device (Drag, draw, and etc)
5) I am trying to run UI program (storyboard) in framebuffer distro based yocto linux, but it even doesn't move with my mouse. Only keyboard works well so far.
Can anyone help me use touchscreen input in UI program?
Hi HUN
from dts file egalax_ts is supported on sabre auto board
imx6qdl-sabreauto.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
More details about HannStar lcd with touchscreen (which is used on i.MX6Q NXP
reference boards) can be found on
https://community.nxp.com/message/810313?commentID=810313#comment-810313
One can try sabre auto board demo images from link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------