Dear All,
Currently, I'm designing a power adapter as below:
- Power: 18W - 20W
- 1 USB-Type C port (Support QC4+)
- 1 USB-Type A port (Support QC 2, 3)
I'm using your chipset (TEA19051). But i don't understand how to design this product have two output (1 USB-Type C and 1 USB-Type A) that using one chipset (TEA19051).
Can you help me?
Hi,
You need two outputs with one TEA19051,right?
Sorry that can you tell us where you find some information about one TEA19051 support two channels outputs? I want to make sure I didn't miss something.
Hi,
Thanks for your reply!
I see in the datasheet have some information as below:
Support:
- USB Type-C v.1.3
- USB Power Delivery (USB-PD) 2.0 and 3.0 including Programmable Power Supply
(PPS)
- Supports Qualcomm® QuickCharge™ QC2.0, QC3.0, and QC4+ protocols
- Battery Charging 1.2 (BC 1.2)
So, I want to designing a product that support two channels outputs!
Hi,
Yes,it can support such topology but only can support one channel output.
Hi,
Yes, thank you so much!