Hello, I am new starting with FRDM-KW019032 board, and I have succeeded following the file "SMAC_QUICK_START_GUIDE" to debug the board with IAR 7.80.4 in win10. But I have two trouble as followed:
1. Although I can Download and Debug a smac_connectivity_test demo code with IAR, I found if the board is reset or re-powered, the code I just download is gone, and no software run on it. How can I permanently flash the code to the board?
2. If I just want to flash a binary file to the board, for example "frdmkw01_connectivity_test_eu.bin", the manual says " by simply dragging and dropping the binary image in the mass storage drive", but when I drop the file to MBED drive, the board seems to disconnect and restart, the transmitting was interrupted. Why?
Thank you so much !
Hello,
By any chance, are you working on Windows 10?
Regards,
Estephania
Yes, I am working in windows 10, is it not suitable for frdm-kw019032? Thanks!