MFG tool for mass production

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG tool for mass production

992 Views
nmedisetty
Contributor I

Hi

We would like to use the MFG tool for mass production of our IMX7 device. I edited the UICfg.ini to  use it with four devies

 which can be simultaneously attached to multiple USB ports of the host PC and can be programmed simultaneously.

I am able to programme four devices at a time.

Is there any way to increase this further so that I can programme more devices simultaneously which will be very helpful in mass production.

0 Kudos
1 Reply

645 Views
igorpadykov
NXP Employee
NXP Employee

Hi Naresh

seems mfg tool should be modified to support more devices, sources are available on

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos