HI,
I want to test imx6q-sabresd. The device driver seems to be properly configured.
I want to know if there are test codes.
For example, the test code can transfer the spi data of the imx6 board to another board.
(The data received from the imx6 board can do something else through the test code.
Please help me.
ps. add questions.
Hi kangta
for testing one can use unit tests described in Chapter 9 Unit Tests attached Linux Manual
imx-test
https://source.codeaurora.org/external/imx/imx-test/tree/?h=imx_4.9.88_2.0.0_ga
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------