AnsweredAssumed Answered

Get DCIC driver for yocto linux created with "sumo"

Question asked by Marcos Lopez on Aug 31, 2018

I recently created a linux kernel for arm using yocto with this repository: GitHub - Freescale/fsl-community-bsp-base: BSP base files perfoming the following steps (I didn't modified the conf provided by default):

- repo  https://github.com/Freescale/fsl-community-bsp-base.git

- repo sync

- MACHINE=imx6qdlsabresd DISTRO=fslc-x11 source setup-environment build

- bitbake meta-choolchain

And I got the a the kernel 4.15.7

So far it is fine for me but I can't find the dcic driver files.

Do I need to build the yocto distro using other parameters or the dcic should be added with patches?

Thanks for any help!

Outcomes