XEP100 - Is there anything special about PIT channels 4-7 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XEP100 - Is there anything special about PIT channels 4-7 ?

1,093 Views
Pedro_
Contributor III
Hi all,
 
I am currently using PIT channels 0-4 with xgate, but I haven't been able to get interrupts out of channels 4-7.
 
I can see the timeout flags in PITTF getting set as expected for these channels, but no thread is executed.
 
I tried handling the interrutps using the H12 and Xgate cores but nothing.
 
Are these vector addresses correct?
H12: 0x58 - 0x5E
XGT: 0x2C - 0x2F
 
Anything special about these channels?
 
Thanks


Message Edited by Pedro_ on 2008-11-27 01:17 PM
Labels (1)
0 Kudos
1 Reply

260 Views
Pedro_
Contributor III
My mistake,
the interrupt module was not set correctly for addresses 0x50 to 0x5E.
 
Thanks
0 Kudos