Hi all,
I am using imx8mqevk boardv3 development board Release - Linux 4.9.88_2.0.0_ga. wireless interface is missing. So on checking dmesg, I can see that bcmdhd_wlan probing fails. see below log.
[ 2.448885] bcmdhd_wlan@0 supply wlreg_on not found, using dummy regulator
[ 2.449100] bcmdhd_wlan: probe of bcmdhd_wlan@0 failed with error -1
So its a pre-build, hence wifi/bt module should be working directly, what may be the solution to start wifi and bluetooth both.
Hi sandeep
currently Linux L4.9.51 is "GA" officially supported release for i.MX8M and
supports QCA6174A, its usage can be found in documentation below
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Actually we are planning to use Release - Linux 4.9.88_2.0.0_ga only for our custom board development. So may I know, how can we support QCA6174 for this release. Or may I know when will NXP officially releases 4.9.88_2.0.0_ga with full working stack.