P2020 DDR2 update to DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 DDR2 update to DDR3

515 Views
billy_huan
Contributor I

Hi NXP:

Our new design will update P2020's memmory from DDR2 to DDR3, but there is no DDR reset of P2020 mmu for DDR3. 

So, how can I deal with the reset signal without CPLD?

Is it available which being connectted to Hreset directly?

BillyHuan

B.R.

0 Kudos
1 Reply

366 Views
ufedor
NXP Employee
NXP Employee

As  DDR3 reset it is possible to use a copy of the reset signal going to the P2020's HRESET input.

0 Kudos