AnsweredAssumed Answered

I2C on T2080 RDB

Question asked by Monali Haware on Aug 26, 2018
Latest reply on Aug 28, 2018 by Pavel Chubakov

this is regarding T2080RDB I2c interface.
I believe that ccb clock is 600KHZ according to the init file. i wamt to do ask the following-

1. i2c maximum frequency is 400KHz so is it okay to program i2cfdr=0x06 (for 360.576KHz) or 0x29 (for 390KHz)

2. ADT7481 datasheet says that it's device address is 1001100(0x4c) but the user guide says 0x40. WHich is correct?

3. is it correct to program i2cdr as 10011000 for START ( "1001100" + '0' for 0x4c as device address for an instance) ?

Outcomes