AnsweredAssumed Answered

Advice to have quickly a K60 with Ethernet Udp/Tcp and Flash driver

Question asked by arnogir on Aug 27, 2018
Latest reply on Aug 27, 2018 by Mark Butcher

Hello,

 

We need to develop a bootloader for the K60 via the Ethernet (with BootP protocol).

Currently, I'm using the USB bootloader provided by Freescale.

 

Then, Are they a fast option to dispose (without need MQX) an application with the layer Ethernet to receive and send UDP/TCP frame, and then a Nandflash driver?

 

I think there are KDSK, with MCUexpresso? Or other? Are they some exempled? (I already use the MQX Ethernet stack with KDS, but not flash driver).

 

Thank

Outcomes