AnsweredAssumed Answered

set input pin failed in S9ZVL16CLC

Question asked by Li Yinwei on Aug 23, 2018
Latest reply on Sep 4, 2018 by Alice_Yang

Hello!

I use S9ZVL16CLC(32pin) MCU in PE in CW 11.0 and my problem is I can't set pin as any mode related to input, even the normal input mode. But I can set as output mode in the relevant pin successfully in S9ZVL16CLC. And I can set input and output mode normally in S9ZVL32VLF(48pin) on the TRK-S12ZVL board. It's so werid.

Does anyone know the reason?

Thanks for anyone replying.

Outcomes