Multi Core Project M4-M0 and a shared project for M4 and M0 core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Core Project M4-M0 and a shared project for M4 and M0 core

488 Views
anon-92c7959f22
Contributor I

Hello,

i have a workspace with a multi-core setup (C, baremetal) for a LPC 4337.

- Project_M0

- Project_M4

- lpc_chip_43xx

- lpc_chip_43xx_m0

However, i have some code that i need in Project_M0 and also in Project_M4.

Is it possible to create a new project "Cortex_Shared"?

The project/folder or whatever, should contain includes/sources that i need in both projects for M4 and M0?

I tried the project wizard, but with that i need to choose between the core.

Any ideas?

Thx

Tags (2)
0 Kudos
1 Reply

393 Views
lpcxpresso_supp
NXP Employee
NXP Employee

It sounds like you want to use "linked resources". The following post should provide you with the necessary information:

https://community.nxp.com/message/1024759?commentID=1024759#comment-1024759 

Regards,

MCUXpresso IDE Support

0 Kudos