Dear All,
I have a question about LPC1788 RTC's General purpose registers 0-4, I write 1 to General purpose registers 0 , then power off(without battery powered) , General purpose registers 0 value changed to 0 after power on.
the user manual said : These registers can be used to store import information when the main power supply is off . It seems that General purpose registers can not store information without main power supply & battery power supply?
Hi,
The RTC block includes 20 bytes of battery-powered backup registers, allowing system status to be stored when the rest of the chip is powered off. Battery power can be supplied from a standard 3 V Lithium button cell.
I hope this clarifies.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------