AnsweredAssumed Answered

Adding rc.local in image for ls1012afrdm (QorIQ-SDK-V2.0-20160527-yocto)

Question asked by Minal Nemade on Aug 20, 2018
Latest reply on Aug 21, 2018 by Pavel Chubakov

Hi,

I want to add rc.local package in ls1012aFrdm board. So I tried CORE_IMAGE_EXTRA_INSTALL += "fsl-rc-local" in conf/local.conf file. But I faced with problem, I am not getting fsl-rc-local.bb in the image downloaded and also below error message

 

$ bitbake fsl-image-core
Loading cache: 100% |###########################################################################################################| ETA:  00:00:00
Loaded 3438 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'fsl-rc-local' (but /home/nntechsol/source/yacto/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'fsl-rc-local' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['fsl-rc-local']
ERROR: Required build target 'fsl-image-core' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-core', 'fsl-rc-local']

 

So please suggest how to append this features to image for ls1012afrdm.

 

Thansk

 

Best Regards

Minal

Outcomes