Hi,
I am using MKL15Z128CAD4R MCU. I want to write some data to flash. How should I do this? please help. I tried to find online help but couldn't get any help.
Hi,
I am using MKL15Z128CAD4R MCU. I want to write some data to flash. How should I do this? please help. I tried to find online help but couldn't get any help.
Hi,
I would recommend to check and download MCUXpresso SDK software package for KL15 chip.
You could find the [pflash] demo about Flash operation(sector erase/program) with below path:
..\MKL15Z64xxx4\boards\frdmkl25z\driver_examples\flash\pflash
Wish it helps.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Mike for your help.
I have used the same code as you have mentioned above but could not write to flash.
Below Function does not write the data on flash address.
result = FLASH_Program(&s_flashDriver, destAdrss, s_buffer, sizeof(s_buffer));
My observations are, In this function there is variable to write the src buffer to flash register i.e kFCCOBx[].
Ideally it should get updated by src buffer as kFCCOBx[0] = *src++;
I am writing 'a' to the src buffer But it shows constant value as 536883200 instead of 'a'.
Hi,
I don't receive any bug report about MCUXpresso SDK flash driver.
Please check below table, the Flash address must be longword aligned (Flash address[1:0] = 00).
And what's the result value when you called the FLASH_Program() function?
result = FLASH_Program(&s_flashDriver, destAdrss, s_buffer, sizeof(s_buffer));
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mike,
It worked for me. But I have to modify the function as:
//---------------------------------------------------------------------------------------------------------------------
void BOARD_BootClockRUN(void)
{
1. /* Set the system clock dividers in SIM to safe value. */
2. CLOCK_SetSimSafeDivs();
3. /* Initializes OSC0 according to board configuration. */
4. //CLOCK_InitOsc0(&oscConfig_BOARD_BootClockRUN);
5. CLOCK_SetXtal0Freq(oscConfig_BOARD_BootClockRUN.freq);
6. /* Configure FLL external reference divider (FRDIV). */
7. CLOCK_CONFIG_SetFllExtRefDiv(mcgConfig_BOARD_BootClockRUN.frdiv);
8. /* Set MCG to PEE mode. */
9. //CLOCK_BootToPeeMode(kMCG_OscselOsc,kMCG_PllClkSelPll0,&mcgConfig_BOARD_BootClockRUN.pll0Config);
10. /* Configure the Internal Reference clock (MCGIRCLK). */
11. CLOCK_SetInternalRefClkConfig(mcgConfig_BOARD_BootClockRUN.irclkEnableMode,
12. mcgConfig_BOARD_BootClockRUN.ircs,
13. mcgConfig_BOARD_BootClockRUN.fcrdiv);
14. /* Set the clock configuration in SIM module. */
15. CLOCK_SetSimConfig(&simConfig_BOARD_BootClockRUN);
16. /* Set SystemCoreClock variable. */
17. SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;
}
//--------------------------------------------------------------------------------------------------------------------
It works only if I remove line no 4 and 9.
Regards,
Shrek
Hi Shrek,
I think the below code with the issue to set Bus clock & Flash clock to 24MHz:
The correct clkdiv1 should be: 0x10030000U.
Could you try that setting with KL15 chip?
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mike,
I have tried above settings too but the code goes inti infinite loop at following function,
//---------------------------------------------------------------------------------------------------------------------
void CLOCK_InitOsc0(osc_config_t const *config)
{
uint8_t range = CLOCK_GetOscRangeFromFreq(config->freq);
OSC_SetCapLoad(OSC0, config->capLoad);
OSC_SetExtRefClkConfig(OSC0, &config->oscerConfig);
MCG->C2 = ((MCG->C2 & ~OSC_MODE_MASK) | MCG_C2_RANGE(range) | (uint8_t)config->workMode);
if ((kOSC_ModeExt != config->workMode) && (OSC0->CR & OSC_CR_ERCLKEN_MASK))
{
/* Wait for stable. */
while (!(MCG->S & MCG_S_OSCINIT0_MASK)) //goes to infinite loop here.
{
}
}
}
//---------------------------------------------------------------------------------------------------------------
Regards,
Shrej
Hi Shrej,
Could you share the KL15 board clock schematics for double check?
I don't meet any issue during test with FRDM-KL25Z board.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mike,
I have created a code from https://mcuxpresso.nxp.com/en/clock and it worked for me.
//-----------------------------------------------------------------------------------------------------------------
#include "clock_config.h"
/*******************************************************************************
* Definitions
******************************************************************************/
#define MCG_IRCLK_DISABLE 0U /*!< MCGIRCLK disabled */
#define MCG_PLL_DISABLE 0U /*!< MCGPLLCLK disabled */
#define OSC_CAP0P 0U /*!< Oscillator 0pF capacitor load */
#define OSC_ER_CLK_DISABLE 0U /*!< Disable external reference clock */
#define SIM_OSC32KSEL_OSC32KCLK_CLK 0U /*!< OSC32KSEL select: OSC32KCLK clock */
#define SIM_PLLFLLSEL_MCGFLLCLK_CLK 0U /*!< PLLFLL select: MCGFLLCLK clock */
#define BOARD_BOOTCLOCKRUN_CORE_CLOCK 48000000U /*!< Core clock frequency: 48000000Hz */
/*******************************************************************************
* Variables
******************************************************************************/
/* System clock frequency. */
extern uint32_t SystemCoreClock;
/*******************************************************************************
* Code
******************************************************************************/
/*FUNCTION**********************************************************************
*
* Function Name : CLOCK_CONFIG_FllStableDelay
* Description : This function is used to delay for FLL stable.
*
*END**************************************************************************/
static void CLOCK_CONFIG_FllStableDelay(void)
{
uint32_t i = 30000U;
while (i--)
{
__NOP();
}
}
/*******************************************************************************
************************ BOARD_InitBootClocks function ************************
******************************************************************************/
void BOARD_InitBootClocks(void)
{
BOARD_BootClockRUN();
}
/*******************************************************************************
********************** Configuration BOARD_BootClockRUN ***********************
******************************************************************************/
/*******************************************************************************
* Variables for BOARD_BootClockRUN configuration
******************************************************************************/
const mcg_config_t mcgConfig_BOARD_BootClockRUN =
{
.mcgMode = kMCG_ModeFEI, /* FEI - FLL Engaged Internal */
.irclkEnableMode = MCG_IRCLK_DISABLE, /* MCGIRCLK disabled */
.ircs = kMCG_IrcSlow, /* Slow internal reference clock selected */
.fcrdiv = 0x1U, /* Fast IRC divider: divided by 2 */
.frdiv = 0x0U, /* FLL reference clock divider: divided by 1 */
.drs = kMCG_DrsLow, /* Low frequency range */
.dmx32 = kMCG_Dmx32Default, /* DCO has a default range of 25% */
.pll0Config =
{
.enableMode = MCG_PLL_DISABLE, /* MCGPLLCLK disabled */
.prdiv = 0x0U, /* PLL Reference divider: divided by 1 */
.vdiv = 0x0U, /* VCO divider: multiplied by 24 */
},
};
const sim_clock_config_t simConfig_BOARD_BootClockRUN =
{
.pllFllSel = SIM_PLLFLLSEL_MCGFLLCLK_CLK, /* PLLFLL select: MCGFLLCLK clock */
.er32kSrc = SIM_OSC32KSEL_OSC32KCLK_CLK, /* OSC32KSEL select: OSC32KCLK clock */
.clkdiv1 = 0x10000U, /* SIM_CLKDIV1 - OUTDIV1: /1, OUTDIV4: /2 */
};
const osc_config_t oscConfig_BOARD_BootClockRUN =
{
.freq = 0U, /* Oscillator frequency: 0Hz */
.capLoad = (OSC_CAP0P), /* Oscillator capacity load: 0pF */
.workMode = kOSC_ModeExt, /* Use external clock */
.oscerConfig =
{
.enableMode = OSC_ER_CLK_DISABLE, /* Disable external reference clock */
}
};
/*******************************************************************************
* Code for BOARD_BootClockRUN configuration
******************************************************************************/
void BOARD_BootClockRUN(void)
{
/* Set the system clock dividers in SIM to safe value. */
CLOCK_SetSimSafeDivs();
/* Set MCG to FEI mode. */
#if FSL_CLOCK_DRIVER_VERSION >= MAKE_VERSION(2, 2, 0)
CLOCK_BootToFeiMode(mcgConfig_BOARD_BootClockRUN.dmx32,
mcgConfig_BOARD_BootClockRUN.drs,
CLOCK_CONFIG_FllStableDelay);
#else
CLOCK_BootToFeiMode(mcgConfig_BOARD_BootClockRUN.drs,
CLOCK_CONFIG_FllStableDelay);
#endif
/* Configure the Internal Reference clock (MCGIRCLK). */
CLOCK_SetInternalRefClkConfig(mcgConfig_BOARD_BootClockRUN.irclkEnableMode,
mcgConfig_BOARD_BootClockRUN.ircs,
mcgConfig_BOARD_BootClockRUN.fcrdiv);
/* Set the clock configuration in SIM module. */
CLOCK_SetSimConfig(&simConfig_BOARD_BootClockRUN);
/* Set SystemCoreClock variable. */
SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;
}
//---------------------------------------------------------------------------------------------------------------------------------
Regards,
shrej
Hi,
I would recommend to check and download MCUXpresso SDK software package for KL15 chip.
You could find the [pflash] demo about Flash operation(sector erase/program) with below path:
..\MKL15Z64xxx4\boards\frdmkl25z\driver_examples\flash\pflash
Wish it helps.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------