I am trying to generate PWM to control PMSM Motor with three phase inverter.
Configuration for each of the PWM Module A is given below(Using eFlexPWM).
Sub Module 0 - Complementary PWM
Clock source - IPBus Clock
Local Reload
Full cycle reload
PWM Reload at every opportunity.
Sub Module 1 - Complementary PWM
Clock source - Sub Module 0 Clock
Master Reload
Master Sync
Full cycle reload
PWM Reload at every opportunity.
Sub Module 2 - Complementary PWM
Clock source - Sub Module 0 Clock
Master Reload
Master Sync
Full cycle reload
PWM Reload at every opportunity.
I am using ADC End of Conversion Interrupt(with PWM Sync for Triggering an ADC) to reload PWM Registers.
With Sub Module 0, If i make it as independent PWM Mode, I can see PWM on the Pins.
But same does not work with other modules.
I have been working with eFlex PWM from past 3 Years with DSC Series Controller and didn't find any problem to generate PWM for three phase inverter. But, The same couldn't work with Kinetis Controller MKV46F256VLL. Can anyone tell where i am going wrong?.
Any help is appreciable.
Hi,
Could you check with below document, which using PWM sub-module in complementary mode.
Two or more eFlexPWM synchronization for KV4x, KV5x, MC56F84xxx and MC56F82xxx
Wish it helps.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------