Flash programming, and other related functions, are supported in several different ways:
• For details of USART In-System Programming, see Section 5.4.
• For details of I2C and SPI In-System Programming, see Section 5.5.
• For details of In-Application Programming, see Section 5.6.
• For details of USB programming, see Chapter 41 “LPC546xx USB ROM API”. The boot loader version can be read by ISP/IAP calls (see Section 5.4.5.13 or Section 5.6.6).
Have a great day, Sol
----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! -----------------------------------------------------------------------------------------------------------------------
Hi,
You can check this in the user manual for the LPC54608, chapter 5.
https://www.nxp.com/docs/en/user-guide/UM10912.pdf
Flash programming, and other related functions, are supported in several different ways:
• For details of USART In-System Programming, see Section 5.4.
• For details of I2C and SPI In-System Programming, see Section 5.5.
• For details of In-Application Programming, see Section 5.6.
• For details of USB programming, see Chapter 41 “LPC546xx USB ROM API”. The boot loader version can be read by ISP/IAP calls (see Section 5.4.5.13 or Section 5.6.6).
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------