Hi,
I have faced this problem earlier while doing flash programming through Tools->Flash programmer.
At that time, the target memory buffer address range is conflicting with the processor's exception vector table. Once I changed the target memory buffer address range, the problem got resolved.
Hi,
I am having problem as likeyou as follow,
CCSProtocolPlugin::Could not connect to the requested core core #0."
Build Environment : LTIB(Linux Target Image builder).
Processor : MPC8315eRDB
Linux version : 2.6.24.3-rt3
debugging Environment : Codewarrior for Power Architecture Linux Platform edition
Host PC OS : Fedora Core 5
I am having problem in connecting the target board with Codewarrior using USB TAB.
When ever If I pressed Debug tab or run tab or connect tab under debug option It is displaying message as CCSProtocolplugin::Could not connect to requested core core #0.
Please help me to resolve the problem.
Hi All,
I am having the exact same problem with the MPC8641D, "ccs_error=39". Did you come up with a solution to resolve this problem? or have some directions?
Many Thanks,
Mike