AnsweredAssumed Answered

S32DS and IAR toolchain support SDK

Question asked by Mac Kim on Aug 16, 2018
Latest reply on Sep 25, 2018 by Rares Vasile

Hello.

 

To create IAR SDK project, do I need to install IAR 7.x?

 

I just installed IAR 8.x at my laptop.

but, if I create S32DS project based on 'IAR 8.x toolchain' there is no selectable SDK list.

if I create 'IAR 7.x- SDK' project, S32DS shows error finding IAR 7.x toolchain. (But, I didn't installed it.)

 

So, I wonder I must install IAR 7.x to create SDK project at S32DS.

Added with it, is there approximate schedule to support IAR 8.x SDK?

 

Best Regards,

Mac.

Outcomes