AnsweredAssumed Answered

Ethernet compliance testing of Linux board based on iMX6UL & KSZ8041NLI

Question asked by Ghanshyam Dudhat on Aug 15, 2018
Latest reply on Aug 19, 2018 by igorpadykov

Dear Sir,

 

We are testing our product for Ethernet compliance testing through DSO Pre-compliance test module but as per test procedure need a test firmware with predefined test packet,

refer the required format -  scrambled, MLT-3 encoded /I/ code-groups (this is a 3-level pseudo-random bit sequence).

Can any one help us to create test application or share with us the application note or test firmware (Linux operating System) to perform the mentioned test.

 

Refer the below NXP and Mirochip PHY part details –

NXP Processer: iMX6UL

Ethernet PHY : KSZ8041NLI-TR

 

 Ethernet section schematic :

 

Attachments

Outcomes