AnsweredAssumed Answered

DEVKIT-MPC5744P CAN Connections

Question asked by Mirac Gulgonul on Aug 14, 2018
Latest reply on Aug 30, 2018 by Martin Kovar

I'm having trouble with making the physical connections for CAN communication on the DEVKIT-MPC5744P board. Let's say CAN Bus 0 is transmitting and CAN Bus 1 is receiving a message. I have set CAN Bus 0 Receive Pin to B1 and Transmit to B0. Similarly CAN Bus 1 has A15 for receive and A14 for transmit. Which jumper connections should I make to enable data transfer between these two modules ? Where should I connect the CAN0H and CAN0L pins ? I don't see any high or low pins for CAN1, only receive and transmit.

Outcomes