Dear All:
I try to build S32DS Project from Example by the S32DS.Vision.2.0 IDE with the VisionSDK_S32V2_RTM_1_1_1. But when I build the project,the cross tool error is "aarch64-linux-gnu/bin/ld.exe: cannot find sequencer.a".
I try to find it in the s32v234sdk directory,but I only find the similar one which is libsequencer.a,and its format is elf32.
I try to rename the libsequencer.a to sequencer.a and add it to my cross tool's lib dir,but the error is " skipping incompatible d:/nxp/s32ds_vision_v2.0/cross_tools/gcc-aarch64-linux-gnu-4_9/bin/../lib/gcc/aarch64-linux-gnu/4.9.3\sequencer.a when searching for sequencer.a"
I check the other lib such as libh264decdrv.a, it's format is elf64. So, how can I get the correct "sequencer.a" which is compatible with the S32V234 VSDK-RTM1.1.1?
Solved! Go to Solution.
Hi,
can you please check your previous VSDK versions list again? Let me know if it is updated now. Thanks.
Jiri
Hi,
unfortunately vision VSDK RTM v1.1.1 is not compatible with S32DS Vision v2.0 example projects and will not work correctly. You have two options - you can use the very same example from SDK delivered with 32DS Vison v2.0 installation (RTM v1.0.1).
Or you can build example - part of VSDK RTM v1.1.1 - from command line. Just start msys32 shell (runshell.cmd located in [YOUR_VSDK_INSTALL_PATH]\S32DS_Vision_v2.0\S32DS\s32v234_sdk\ ) go to demos/isp/isp/isp_h264dec_single_stream/build-v234ce-gnu-linux-d/ and run
make allsub
command.
You got the .elf file which you can run on your EVB (with Linux).
Hope it helps.
Jiri
Thank you, Jiri. But can you tell me where can I download the VSDK RTM v1.0.1?
I can only find the 1.1.1 version in the NXP Software & Support.
Hi,
I just noticed that your screenshots are from our web pages and it looks like that in your list is not VSDK RTM 1.0.1. Did you try to Product Search - SW32V23_VSDK001_RTM_1_0_1 ?
Jiri
Hi,
I just followed your steps by clicking the https://nxp.flexnetoperations.com/control/frse/index and Go to Automotive SW - Vision Software.
Then ,I pushed the "previous button",but the web page below was different from yours, it just showed 1.1 verison.
Hi,
can you please check your previous VSDK versions list again? Let me know if it is updated now. Thanks.
Jiri
Hi Jiri,
Can you tell me which Auto Linux BSP Version is compatible with the VSDK RTM1.0.1?
Now I use the BSP17.0, and the linux rootfs.tar of the VSDK RTM1.0.1 couldn't be compatible with the Image and dtb created by Linux BSP 17.0.
Hi,
Thank you, it updated. And I can get the VSDK RTM1.0.1 in the previous VSDK versions list.
Hi,
this VSDK version is part of S32DS Vision v2.0 installation (located in [YOUR_S32DS_INSTALL]\S32DS_Vision_v2.0\S32DS\s32v234_sdk\ )
Jiri
Hi,Jiri
I reinstall S32DS_Vision_Win32_v2.0_b170913_redrop03.exe,but this VSDK version is not a part of S32DS Vision v2.0 installation. I counld not find the VSDK vesion in that dir, and I open the Release_Notes.pdf, it said that I need to copy the vsdk to the S32DS folder. How can I get the compatible VSDK or the S32 DS?
Hi,
Sorry, I have different build (older) number already with VSDK. So - in this case - you can find older VSDK versions here:
https://nxp.flexnetoperations.com/control/frse/index
Go to Automotive SW - Vision Software
Select Previous
And get the version RTM v1.0.1
Hope it helps.
Jiri