Hi,
I have a T2080 booting in core 0 (with JTAG attached), but I would like to know how to enable secondary cores (1, 2 and 3). Do I need to set a physical jumper? I found a register to disable cores but not for enabling.
The target is using Minimon instead of uboot.
Thanks in advance.
I assume that you have CodeWarrior and CodeWarrior TAP.
Please create a bareboard project, in the Processing Model configuration panel , please select Core index as you required.
Please open CodeWarrior launch configuration from Run->Debug Configurations-><project>_RAM_<processor>_Download, please select multicores at Target Settings, then connect to the target board, the CodeWarrior demo program will be executed on each core.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
启动linux还是rtos还是裸机main()?