HI,FSL,In my item,we think the hdmi clock output is error,we check the clock is :
clk[IMX6QDL_CLK_HDMI_ISFR] = imx_clk_gate2("hdmi_isfr", "pll3_pfd1_540m", base + 0x70, 4);
is the hdmi clock source "pll3_pfd1_540m"?
Hi yi
yes seems this is correct as from Table 18-3. System Clocks, Gating, and Override
i.MX6DQ Reference Manual isfrclk has clock source as video_27m_clk_root and it has
source as "pll3_pfd1_540m" according to
Figure 18-3. Clock Tree - Part 2, VIDEO_27M_CLK_ROOT,
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
in my code, the clock setting is below:
clk[IMX6QDL_CLK_HDMI_ISFR] = imx_clk_gate2("hdmi_isfr", "pll3_pfd1_540m", base + 0x70, 4);
but the hdmi clock is not booting in kernel,why?