hardware: i.mx6q
software: yocto 3.14.28
The ITU-R BT656 specifies that the nominal
range for video should be restricted to values between 16 and
235 for luma and 16 and 240 for chroma.
The values is out of the range after deInterlacing by IPU-VDIC.
How to control the rang for IPU-VDIC output?
one can change it in the IPU source code, more detailed information, pls refer to the document as below:
iMX6 camera patch to support CSI->VDI->IC->MEM and CSI->VDI->MEM capture