AnsweredAssumed Answered

MCUXpresso v10.2.0.759 - hangs at 2% when debugging

Question asked by Mathieu Borderé on Aug 8, 2018
Latest reply on Aug 10, 2018 by Erich Styger

Setup is an i.MX RT1050 board connected with a j-link Segger interface running on a Windows 10 machine.

 

After a couple of debug sessions, launching a debug session will hang at 2% completion and stay there for easily 60+ seconds. Restarting MCUXpresso solves the issue temporarily, untill it returns after launching a handful of debug sessions.

 

Also see this topic https://community.nxp.com/thread/480133 where I describe the same issue for MCUXpresso 10.1.1.606, however in that version the problem is even more accute it seems. I have already tried the latest version of MCUXpresso, but the problem remains.

 

Other members in my team face the same problem and it can be quite frustrating at times. 

 

Can I enable some logging or provide certain additional information to more easily identify the source of this problem?

 

Any help is greatly appreciated,

Kind regards,

Mathieu

Outcomes