Our product is using imx6qplus and Android 7.1.2.
We want to do eMMC boot.
We use "mfgtoolsL4.9.11_1.0.0" to write eMMC ,but follow error log is come out.
########################
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid
########################
Do the file "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" can't be used directly?
How to fix this problem?
Solved! Go to Solution.
I check config about conig of u-boot .CONFIG_ENV_IS_NOWHERE isn't defined.
I define this config and build u-boot.imx again.
The Ramdisk image can be loaded.
I check config about conig of u-boot .CONFIG_ENV_IS_NOWHERE isn't defined.
I define this config and build u-boot.imx again.
The Ramdisk image can be loaded.