LPC824M201JHI33 use without oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824M201JHI33 use without oscillator

390 Views
daniel2
Contributor I
0 Kudos
1 Reply

320 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Daniel Brown

In the user manual of the LPC824 (https://www.nxp.com/docs/en/user-guide/UM10800.pdf) under section 5.3.2 you can find the following information. 

pastedImage_4.png

So, you can definitely use the internal oscillator as the main clock. The development board for the LPC824 (LPCXpresso824-MAX Board for LPC82x family MCUs|NXP ) actually uses the IRC in all the examples that we provide (Code Bundle, LPCOpen and SDK) as the input for the PLL and the output of the PLL is the source of the main clock.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos