AnsweredAssumed Answered

Questions about MMZ09332BT1

Question asked by Guilherme Theis on Aug 7, 2018

Hello,

I have been testing the MMZ09332BT1 and I will be using it in my application, I did some stress testing but I was not able to verify the PDC (ended up damaging the circuit in the stress testing). So here are my questions:

 

1) I would like to know if I can ground my PDC connection in my board design, thus making my PA to be biased all the time and then use an enable/disable for my VDD (which I can easily do with the DC/DC converter I am using).

 

2) I would like to know how to properly set a thermal dissipation in my board/for my PA

 

3) I would like to know if there is anyway I could get the information used to generate the evaluation board for this PA (433 MHz), about the stackup used for the board, the dielectric material, etc.

 

Best regards,

 

Guilherme Theis

Outcomes