special registers in Registers view for LinkServer debug sessions still show incorrect values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

special registers in Registers view for LinkServer debug sessions still show incorrect values

734 Views
leleguan
Contributor I

In the changelog of MCUXpresso IDE V10.2.1, it states the following bug fix.

  • Fixed issue with display of PriMask, BasePri, FaultMask and Control special registers in Registers view for LinkServer debug sessions. 

Unfortunately, I found that the issue is not fixed, at least for Linux. Does anyone have the same issue?

Labels (1)
Tags (1)
0 Kudos
2 Replies

550 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Can you please clarify the exact behaviour you are seeing please, along with the target MCU and debug probe being used.

Regards,

MCUXpresso IDE Support

0 Kudos

550 Views
leleguan
Contributor I

Thanks for the reply.

The control register is always 0 even when I have set the SPSEL bit, and PRIMASK is 2, which should be an invalid status.

I work on Ubuntu 18.04. I use an NXP FRDM-k66 board, which is equipped with an M4 core. I used the default IDE LinkServer (DAPLink CMSIS-DAP) on the NXP's OpenSDA interface.

I temporarily switched to v10.1.1 which works fine.

Regards,

Le

0 Kudos