Hi,
On the custom hardware we are using MCIMX6Y2CVM08AA processor. After power ON, all the voltage levels are fine except the VDDA_ADC_3P3 which is 3.9V so i remove the power input to this particular voltage input pin L13 (VDDA_ADC_3P3) but still see a voltage level of 3.9V on this pin (without power connected to this particular pin).
Can you please suggest us any debugging steps or a solution if this is a known issue.
Thanks.
Hello,
verify Your design, if it meets the Hardware Development Guide :
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf
Also use
https://community.nxp.com/docs/DOC-129659
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!