S32K flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K flash

1,003 Views
luo812
Contributor I

How config S32K148 P_Flash write unit to 4 Byte(in PROGRAM_LONGWORD mode)?when I modity the macro define  FEATURE_FLS_PF_BLOCK_WRITE_UNIT_SIZE ,FEATURE_FLS_DF_BLOCK_WRITE_UNIT_SIZE from 8 to 4 in S32K148_features.h ,but the func FLASH_DRV_Program will return STATUS_ERROR,please help me,thanks!

0 Kudos
1 Reply

685 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The Flash on S32K1xx can be written in 8-byte phrases.

Please refer to Section 36.5.11.4 Program Phrase command, RM rev.8.

Regards,

Daniel

0 Kudos