About SSI errata ERR008990.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About SSI errata ERR008990.

Jump to solution
778 Views
takayuki_ishii
Contributor IV

Hello community, 

In errata of i.MX6 (IMX6DQCE), it have errata of useing SSI in i2s mode function.

It have a software workaround in Linux BSP release imx_3.10.1_1.1.0_ga.

I think that this commit applies.

ENGR00273838-4 ASoC: fsl: Enable dual-fifo mode as default 

But newer version of Linux BSP have no implement about it.

Is this software workaround are integrated in newer version of Linux BSP?

Best regards,

Ishii.

Labels (3)
Tags (2)
0 Kudos
1 Solution
549 Views
art
NXP Employee
NXP Employee

The workaround should be already integrated into the later versions of the Linux BSP.


Have a great day,
Artur

View solution in original post

0 Kudos
3 Replies
550 Views
art
NXP Employee
NXP Employee

The workaround should be already integrated into the later versions of the Linux BSP.


Have a great day,
Artur

0 Kudos
549 Views
takayuki_ishii
Contributor IV

Hello Artur,

Thank you for your answer.

How about android BSP?

Our customer use Android N 7.1.2_2.0.0, it is Linux 4.9.17 kernel based on the Linux BSP L4.9.11 ga.

Is it integrated this workaround?

Best regards,

Ishii.

0 Kudos
549 Views
takayuki_ishii
Contributor IV

Hello art

I'm very sorry my stingy question.

Is it integrated to Android BSP?

Our customer use an Android BSP N7.1.2_2.0.0.

Best regards,

Ishii.

0 Kudos