AnsweredAssumed Answered

Input Capture and Output Compare By using S12ZVML31

Question asked by Frank Kong on Aug 2, 2018
Latest reply on Aug 14, 2018 by lama

@Alice_Yang 

Hello, 

    I,m using s12zvml31 for capture square wave's frequency and duty。Simultaneously, output square wave with the same frequency and specific duty(5% for example). The input frequency is between 10Hz and 1000Hz.

    S12zvml31 only have a Timer0 and my main interrupt cycle is 100us, what can I do to solve this problem?  The main iterrupt cycle has the highest priority.

       My timer's frequency is 625K now. 

Outcomes