Replacement for the 9s08 family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacement for the 9s08 family

479 Views
nasim
Contributor I

Dear Sir

I have number of products developed on the Following ICs

9s08sh32cwl, 9s08sh16cwl, 9s08sh16mctj, 9s08qg8cdte ,9s08qe32 ,9s08qd4

I believe they will not be in production after 2020,Can you please recommend any alternate part that can be used instead of these .I want to make  minimum effort for changes in hardware and software 

Regards

Nasim

0 Kudos
2 Replies

433 Views
b36401
NXP Employee
NXP Employee

Here is a table you can see the longevity of our products:
https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM?&fsrch=1&sr=1&...
You can set Microcontrollers and 8-bit S08 as a filter.
And then you can see some parts with 15 Year longevity as well.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

433 Views
nasim
Contributor I

Dear Victor

Thanks for the prompt response. It is a big help.Can you please confirm if 9s08QG8 is already out of production as I could not find it on the  list.

Regards

Nasim

0 Kudos