AnsweredAssumed Answered

gpu demo not work on x11 mode

Question asked by huo can on Aug 2, 2018

我现在使用yocto的版本是L3.14.52,使用IMX6Q的芯片,

使用下面这个编译命令

DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b imx6q-x11

bitbake fsl-image-qt5

使用该命令生成的uboot image 及rootfs烧写到板子上,进行GPU 测试例程的编译运行出现如下问题

root@freescale /gpu_sdk_v1.00/Samples/GLES2.0/bin/GLES20_X11$ ./01_SimpleTriangle
01_SimpleTriangle: ../common/src/fsl_egl.c:51: fsl_getNativeDisplay: Assertion `eglNativeDisplayType != ((void *)0)' failed.
Aborted

 

但是我使用

$ MACHINE=imx6qsabresd source fsl-setup-release.sh -b imx6q-fb -e fb                 
$ bitbake fsl-image-qt5

生成的uboot image 及rootfs烧到板子上,GPU的测试历程可以正常运行

 

怎么可以在x11中正确运行GPU的测试历程

Outcomes