Hi,
Creating new configuration for processor LPC54606J512.
Selecting one of the signals in FC2 initiates the warning.
How and where to tell the config tool 4.1 about the initialization?
Checked the board LPCXpresso54618.mex which is using FC0-3 and 6,7.
No warnings for FC0-3 but warnings for FC6,7....
Thanks in advance.
oops, paying attention to the peripheral tool solved the warning
Hello Viggo Joergensen,
After configure FC2, the code will be generated automatically in the file peripherals.c and peripherals.h.
Please take a screnshot about your warning and attached your config project .
BR
Alice
Hello Alice,
Still having warnings of a peripheral (ADC0) not initialized.
I’m using just one ad input – ch5.
Pls see the attached screen snips warning and routed pins.
Are you able to help ?
Thanks in advance.
Med venlig hilsen / Kind regards
Viggo Jørgensen
Civilingeniør, Software- / hardwareudvikler
Direkte: +45 87 12 51 09
E-mail: VIJO@tarp.dk<mailto:VIJO@tarp.dk>
<http://www.tarp.dk/nyheder/vi-stoetter-kampen-mod-brystkraeft.html>[www.tarp.dk]<http://www.tarp.dk/>
Fra: Alice_Yang <admin@community.nxp.com>
Sendt: 2. august 2018 11:09
Til: Viggo Jørgensen <VIJO@tarp.dk>
Emne: You have been mentioned by Alice_Yang in Re: Warning: Peripheral FLEXCOMM2 is not initialized in NXP Community
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
You have been mentioned
by Alice_Yang<https://community.nxp.com/people/Alice_Yang?et=notification.mention> in Re: Warning: Peripheral FLEXCOMM2 is not initialized in NXP Community - View Alice_Yang's reference to you<https://community.nxp.com/message/1041420?commentID=1041420&et=notification.mention#comment-1041420>
Hello Viggo,
Please right click this warning, then choose "Initialize ADC0 peripheral":
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Alice,
Thanks for your quick response.
It solved the warning.
I wasn’t aware of the right click menu in that field.
Have a nice day too.
Med venlig hilsen / Kind regards
Viggo Jørgensen
Civilingeniør, Software- / hardwareudvikler
Direkte: +45 87 12 51 09
E-mail: VIJO@tarp.dk<mailto:VIJO@tarp.dk>
<http://www.tarp.dk/nyheder/vi-stoetter-kampen-mod-brystkraeft.html>[www.tarp.dk]<http://www.tarp.dk/>
Fra: Alice_Yang <admin@community.nxp.com>
Sendt: 7. august 2018 11:59
Til: Viggo Jørgensen <VIJO@tarp.dk>
Emne: Re: - Re: Warning: Peripheral FLEXCOMM2 is not initialized
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Warning: Peripheral FLEXCOMM2 is not initialized
reply from Alice_Yang<https://community.nxp.com/people/Alice_Yang?et=watches.email.thread> in MCUXpresso Config Tools - View the full discussion<https://community.nxp.com/message/1043214?commentID=1043214&et=watches.email.thread#comment-1043214>
OK, welcome !
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------