AnsweredAssumed Answered

No valid url for imx-gpu-viv_6.2.4.p0.4-aarch32

Question asked by Moorthy Baskar on Jul 31, 2018

I'm trying to build 32-bit rootfs on imx8mq-evk board by referring 64-bit machine configuration. Created a new machine configuration (imx8mqevk32) for 32-bit with cortexa9thf-neon TUNE SETTINGS where linux kernel provider pointed to "linux-dummy" (boot loader and linux-imx kernel are used from 64-bit build). While building imx-gpu-viv recipe, the source URL points to https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-6.2.4.p0.4-aarch32.bin which is invalid and shows "page not found" on trying from browser. Below given yocto environment is used and it has only one recipe for aarch32.

 

Yocto environment:

Manifest URL - https://source.codeaurora.org/external/imx/imx-manifest.git 

Branch - imx-linux-morty

Manifest - imx-4.9.51-8mq_ga-optee-demo.xml

 

The target build is from 

# source nxp-setup-optee.sh -b build-optee -d imx-xwayland-optee -m imx8mqevk32 -e

# bitbake fsl-image-validation-imx

 

Questions:

1) For 32-bit EGL libraries on iMX8MQ, is this the correct recipe/version to proceed? If so, kindly provide the proper URL for imx-gpu-viv.

2) Is there any pre-built image / rootfs tarball to refer these EGL libraries which is released by NXP?

Outcomes