The question of program EMMC in MCIMX6QP-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The question of program EMMC in MCIMX6QP-SDB

486 Views
yyddddmw
Contributor I

Hello everyone:

We have a development board MCIMX6QP-SDB. And we need to program EMMC. 

According to the instructions, we use L4.9.88 mfgtools. However, this version of mfgtools can not recognize board. 

The following is running screenshots.

1.jpg

And report an error when we send electricity to the board.

The following is error screenshots.

2.jpg

The following is the log of mfgtools.

3.jpg

If we use l3.14.38.6ul verson of mfgtools,  it could recognize board. But when the program EMMC into second step, our board can not be recognized.The following is the screenshots of l3.14.38 mfgtools in second step.

4.jpg

Our host environment is WIN7. The following is the screenshots of host environment.

5.jpg

So, could anyone can tell us how to program the EMMC?

And whether or not it is related to the setting of switch6?

                        Thanks.

0 Kudos
2 Replies

424 Views
art
NXP Employee
NXP Employee

Have you the i.MX6 HID driver properly installed on your host PC? Please check.

Also, please try the earlier MFGtools version, e.g. 4.9.11 or 4.1.15.

Also, what do you mean as the 'switch6'? Please specify.


Have a great day,
Artur

0 Kudos

424 Views
yyddddmw
Contributor I

Sorry to reply a little late.

We do not install i.MAX6 HD driver. Could you give me a link or address to download this driver?

      Thanks

0 Kudos