I have downloaded android_m6.0.1_2.1.0_ga_tool.tar.gz and android_O8.0.0_1.0.0_tools.tar.gz .
1. on win 7 desktop using android_m6.0.1_2.1.0_ga_tool.tar.gz to download images ,it successed.
2. on win 7 desktop using android_O8.0.0_1.0.0_tools.tar.gz to download images ,it failed to notice "No Device Connected".
3.on XP desktop both of them is successful to download images.
Solved! Go to Solution.
The problem have solved . It just is the usb port for PC, changing to use usb2.0 hub .
Thanks!
It maybe caused by the usb port.
1.The board is imx6q .
2.I use the same computer and the same usb port .
Hi,
Could you tell me which flash are you download the images to, emmc or SD card? I will try it on my board and then give you reply.
Have a nice day
Rita
The problem have solved . It just is the usb port for PC, changing to use usb2.0 hub .
Thanks!
OK. Good news.
Which board are you using?