I'm getting the following error out of the box (no changes).
ERROR: python3-3.5.3-r1.0 do_package_qa: QA Issue: /usr/lib/libpython3.5m.so.1.0 contained in package libpython3 requires libc.so.6(GLIBC_2.25)(64bit), but no providers found in RDEPENDS_libpython3? [file-rdeps]
ERROR: python3-3.5.3-r1.0 do_package_qa: QA run found fatal errors. Please consider fixing them.
ERROR: python3-3.5.3-r1.0 do_package_qa: Function failed: do_package_qa
ERROR: Logfile of failure stored in: /home/todd/bluebox/fsl-auto-yocto-bsp/build_ls2084abbminiubuntu/tmp/work/aarch64-fsl-linux/python3/3.5.3-r1.0/temp/log.do_package_qa.11938
ERROR: Task (/home/todd/bluebox/fsl-auto-yocto-bsp/sources/poky/meta/recipes-devtools/python/python3_3.5.3.bb:do_package_qa) failed with exit code '1'
Use Ubuntu 18.04 64bit version for SDK 18.06 building. There are no errors for this command if this Ubuntu is used.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------