AnsweredAssumed Answered

P-Flash and D-Flash

Question asked by Igol Logi on Jul 27, 2018
Latest reply on Jul 30, 2018 by Daniel Martynek

Hi, I'm using the s32k144evb and my application resides in P-Flash since it is to big to be stored directly in RAM ( It seems that if you use the SDK is very difficult to stay in the limits). Since I can't read simultaneously from P-Flash and D-Flash, should I put the D-Flash functions in RAM in order to be able to read it?

 

If yes which is the method permiting me to put only some parts of code in ram?

 

NB:

The defined macro:

START_FUNCTION_DEFINITION_RAMSECTIOn

END_FUNCTION_DEFINITION_RAMSECTION

are defined as void with GCC compiler.

Outcomes