S32 SDK 0.8.4 in S32 Design Studio for ARM v2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 SDK 0.8.4 in S32 Design Studio for ARM v2.0

1,066 Views
mauromarinoni
Contributor I

I've tried to install the different versions of S32 for Linux (i.e., 2018R1, v2.0, v1.3) but I was not able to install the SDK (in particular version 0.8.4 from v2.0). In the end, I was forced to grab it from a Windows installation where the folder is present.

I've missed some options to flag during the installation procedure? Or it's the desired result to avoid the SDK installation in Linux? 

Tags (3)
0 Kudos
1 Reply

936 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately SDK is not supported on Linux host. 

Jiri

0 Kudos